emWin LCD-DMA with LPC1788

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

emWin LCD-DMA with LPC1788

2,099 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by SimonThome on Wed Jun 19 01:39:32 MST 2013

I would prefer if the low-level driver for the LPC1788 utilised the dedicated DMA for the LCD controller, I'm sure this would make it far more efficient.


Are there any plans to impliment this anytime soon?

Labels (1)
0 Kudos
Reply
2 Replies

2,000 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by SimonThome on Sat Jun 22 13:14:01 MST 2013

Nevermind


I missunderstood the LCD DMA 

0 Kudos
Reply

2,000 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by wmues on Fri Jun 21 13:42:27 MST 2013

Simon,


are you joking?


I am very sure that the dedicated DMA is used for all framebuffer-type LCD controller.

0 Kudos
Reply