emWin LCD-DMA with LPC1788

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

emWin LCD-DMA with LPC1788

2,048件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by SimonThome on Wed Jun 19 01:39:32 MST 2013

I would prefer if the low-level driver for the LPC1788 utilised the dedicated DMA for the LCD controller, I'm sure this would make it far more efficient.


Are there any plans to impliment this anytime soon?

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,949件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by SimonThome on Sat Jun 22 13:14:01 MST 2013

Nevermind


I missunderstood the LCD DMA 

0 件の賞賛
返信

1,949件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by wmues on Fri Jun 21 13:42:27 MST 2013

Simon,


are you joking?


I am very sure that the dedicated DMA is used for all framebuffer-type LCD controller.

0 件の賞賛
返信