emWin 5.16 crossworks

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

emWin 5.16 crossworks

1,781 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by wavemed on Thu Aug 23 13:32:21 MST 2012
Why the CrossWorks (CrossStudio) BSP version 5.16 is still not available?
Actually I use the BSP of 5.12 version, can I change only the library file and the include? The downloadable compiled version 5.16 will work correctly with CrossWorks?
Thank you.
Daniele
标签 (1)
0 项奖励
回复
3 回复数

1,717 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by wasabinz on Thu Nov 22 01:49:14 MST 2012
You can use the binary library for LPCexpresso on your Crossworks project. I've tested it on emWin 5.16 and it works out fine.
0 项奖励
回复

1,717 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by kiranbdvt on Thu Nov 22 01:20:14 MST 2012
Dear Wavemed,
I am trying to port emwin on LPC1768 with Crossworks 2. iI have downloaded emwin 5.12 from NXP. there are binary library files for IAR, LPCexpresso and MDK4 but there is no binary library file for crossworks. please let me know how you have ported 5.12 on  crossworks 2? it will help me a lot.
Thanks
Kiran
0 项奖励
回复

1,717 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Henrik on Tue Aug 28 12:29:28 MST 2012
The most recent version that supports CrossWorks is version 5.12. I do not know if CrossWorks is ARM EABI compliant, but if it is you should be able to use the library from version 5.16.
0 项奖励
回复