device ID on LPC5512

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

device ID on LPC5512

2,073件の閲覧回数
JRIIS
NXP Employee
NXP Employee

Hi,
I try to read the device ID with ISP command through UART, but it can't read out the correct device ID number.
The command I send is:
BYTE command1[] = {0x5A, 0xA4, 0x0C,0x00,
0x2C, 0x49, //crc16
0x07, //getproperty
0x00,0x00,0x02, //2 para
0x10,0x00,0x00,0x00, //device id tag 0x10
0x00,0x00,0x00,0x00};

And the data returned from the device is : 0x5A,0xA4,0x08,0x00,0x92,0x68,0xA7,0x00,0x00,0x01,0x3C,0x28,0x00,0x00.

In the datasheet, the device id for LPC5512 is 0xA100370C, is different with the data I received 0x283C.

please help to check.

Thanks.

/Jakob

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

2,060件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello JRIIS,

 

LPC551x/0x doesn't support "get-property 0x10", it is a doc issue.

 

BR

Alice

0 件の賞賛
返信