debug error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

debug error

3,609件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by chidambaramnkl on Mon May 23 01:17:18 MST 2016
While start  debugging i have problem with lpclink 2 debugger tool. the Target board is LPC4357 processor.  Error message given by the debugger is given below. Can any one Help me to get out of this problem

Error in final launch sequence
Failed to execute MI command:
-target-select extended-remote | crt_emu_cm_redlink -msg-port=52143 -g -mi -2 -pLPC4357 -vendor=NXP -ResetScript=LPC18LPC43InternalFLASHBootResetscript.scp -reset= -ProbeHandle=1 -CoreIndex=0 -cache=disable -flash-driver=LPC18x7_43x7_2x512_BootA.cfx
Error message from debugger back end:
Remote communication error.  Target disconnected.: No error.
Remote communication error.  Target disconnected.: No error.
ラベル(1)
0 件の賞賛
返信
3 返答(返信)

3,582件の閲覧回数
lpcware
NXP Employee
NXP Employee
bump
0 件の賞賛
返信

3,582件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by vtw.433e on Mon May 23 01:54:36 MST 2016
Suggest you start with this FAQ:
https://www.lpcware.com/content/faq/lpcxpresso/windows-path-issues
0 件の賞賛
返信

3,581件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by chidambaramnkl on Mon May 23 01:28:28 MST 2016
I here by attached the error message shown by the debugger.
Help me as soon as possible

0 件の賞賛
返信