debug error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

debug error

3,651 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by chidambaramnkl on Mon May 23 01:17:18 MST 2016
While start  debugging i have problem with lpclink 2 debugger tool. the Target board is LPC4357 processor.  Error message given by the debugger is given below. Can any one Help me to get out of this problem

Error in final launch sequence
Failed to execute MI command:
-target-select extended-remote | crt_emu_cm_redlink -msg-port=52143 -g -mi -2 -pLPC4357 -vendor=NXP -ResetScript=LPC18LPC43InternalFLASHBootResetscript.scp -reset= -ProbeHandle=1 -CoreIndex=0 -cache=disable -flash-driver=LPC18x7_43x7_2x512_BootA.cfx
Error message from debugger back end:
Remote communication error.  Target disconnected.: No error.
Remote communication error.  Target disconnected.: No error.
Labels (1)
0 Kudos
Reply
3 Replies

3,624 Views
lpcware
NXP Employee
NXP Employee
bump
0 Kudos
Reply

3,624 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by vtw.433e on Mon May 23 01:54:36 MST 2016
Suggest you start with this FAQ:
https://www.lpcware.com/content/faq/lpcxpresso/windows-path-issues
0 Kudos
Reply

3,623 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by chidambaramnkl on Mon May 23 01:28:28 MST 2016
I here by attached the error message shown by the debugger.
Help me as soon as possible

0 Kudos
Reply