connection failed - Ep(01). Target marked as not debuggable.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

connection failed - Ep(01). Target marked as not debuggable.

2,111 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ranjith Shanbhag on Tue May 19 03:29:37 MST 2015
Hi,


I am using LPC1549 micro controller, not able to detect target for flashing or debug.
I am getting below mentioned error message.

"
LPCXpresso RedlinkMulti Driver v7.6 (Feb  2 2015 09:45:13 - crt_emu_cm_redlink build 253)
============= SCRIPT: LPC15RunBootRomConnect.scp =============
DpID = 2BA01477
RedlinkAPI: Wire Ack Fault - target connected?
RedlinkAPI: Wire Ack Fault - target connected?
RedlinkAPI: Wire Ack Fault - target connected?
RedlinkAPI: Wire Ack Fault - target connected?
Halt on reset vector catch
RedlinkAPI: Wire Ack Fault - target connected?
RedlinkAPI: Wire Ack Fault - target connected?
RedlinkAPI: Wire Ack Fault - target connected?
RedlinkAPI: Wire Ack Fault - target connected?
Halt on watchpoint write of ROMWSCTRL register
RedlinkAPI: Wire Ack Fault - target connected?
RedlinkAPI: Wire Ack Fault - target connected?
============= END SCRIPT =====================================
connection failed - Ep(01). Target marked as not debuggable.ÏRïäŸ
"

Please help me to sort out this.

Regards,
Ranjit
Labels (1)
0 Kudos
Reply
3 Replies

2,020 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Tue May 19 05:58:08 MST 2015
In the first place, read

[list]
  [*]http://www.lpcware.com/content/faq/lpcxpresso/target-marked-not-debuggable
[/list]
Regards,
LPCXpresso Support
0 Kudos
Reply

2,020 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ranjith Shanbhag on Tue May 19 04:14:48 MST 2015
hi,

Board: LPC1549 board(End Product)
Debugger: LPC-Link 2
LPCXpresso version: 7.6.2_326
PC OS: Windows 7
0 Kudos
Reply

2,020 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by R2D2 on Tue May 19 03:43:36 MST 2015
:quest:

Could be useful if you describe your hardware (LPC1549 Board / Debugger / LPCXpresso version / PC OS)

and if you were able to flash it before...
0 Kudos
Reply