brand new

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

brand new

1,427 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by dbarton on Tue Aug 20 15:26:44 MST 2013

I got the IDE up and the Flashmagic working.

Is there a beginner tutorial anywhere about how to get started on very first program?
(I've come from Arduino)


Labels (1)
0 Kudos
Reply
2 Replies

1,415 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by NXP_Paul on Wed Aug 21 06:15:07 MST 2013
1. If you've installed LPCXpresso, then you will find several examples included with the installation in directory "LPCXpresso_5.2.6\lpcxpresso\Examples\NXP\LPC800".
2. There is also an code sample bundles and application notes available for download from: http://www.lpcware.com/node/11538/256
3. Eventually, you will want to change the clock configuration.  You will find an Excel-based "LPC8xx Clock and PLL Configuration Tool" at http://www.lpcware.com/node/11538/256
4. Configuring the switch matrix in the LCP800 is not difficult, but to make it even simpler, you can use the "NXP Switch Matrix Tool for LPC800".  Again, available for download from: http://www.lpcware.com/node/11538/256

With these resources, you should be able to get a good start understanding the LPC800 family.
0 Kudos
Reply

1,415 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by TheFallGuy on Tue Aug 20 23:34:34 MST 2013
Start from one of the examples


Read the getting started guide to get started...
0 Kudos
Reply