ask for LPCXpresso43S67 win10/11 USB driver package

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ask for LPCXpresso43S67 win10/11 USB driver package

7,290 Views
ZJane
Contributor I

1、ask for LPCXpresso43S67 win10/11 USB driver package as it is difficult to connect the www.lpcware.com

2、Can LPCXpresso43S67 work  with WIN11 system?

 

0 Kudos
Reply
14 Replies

7,273 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @ZJane 

I haven't tested with Win11, what about the issue on your side? Please take a screenshot show it.

Please check Device Manger on your PC, whether can recognized the debugger?

How about update debugger firmware on your board?

 

BR

Alice

 

 

0 Kudos
Reply

7,256 Views
ZJane
Contributor I
I didn't see LPC in device manager after install the driver, and it cannot be recognized in the debugger which showed no probes.
What should we do to solve it?
What does "update debugger firmware on your board" mean?
0 Kudos
Reply

7,182 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @ZJane 

 

Please refer to USER GUIDE:

https://www.nxp.com.cn/docs/en/user-guide/UM10946-om13084_88.pdf  

Alice_Yang_0-1686537173356.png

 

BR

Alice

 

0 Kudos
Reply

7,142 Views
ZJane
Contributor I

I tried LPCScrypt, the device cannot be  found.

微信截图_20230613184343.png

0 Kudos
Reply

7,124 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @ZJane 

 

Make sure your board make DFU link as description,  it also mean short 1-2 of JP6 on LPCXpresso4337 board.

Alice_Yang_0-1686711446781.png

 

BR

Alice

 

0 Kudos
Reply

7,098 Views
ZJane
Contributor I

yes, the board make DFU link and connec a micro USB cable to connector J5.

0 Kudos
Reply

7,026 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @ZJane 

If can not enter DFU mode, maybe debugger on board broken.

You can try to use external debugger to test.

 

BR

Alice

0 Kudos
Reply

7,087 Views
ZJane
Contributor I

You can see the error and board connection in the picture below.

 

1.png20230614202031.jpg

0 Kudos
Reply

7,079 Views
frank_m
Senior Contributor III

If you plug it into the host PC, you should see something in the Device Manager.
Does it report any errors ? Are all necessary driver installed / up to date ?

0 Kudos
Reply

7,070 Views
ZJane
Contributor I
I find nothing new in the Device manager, and it report 0 errors.
I have installed the lpc_driver_setup.exe download from NXP website. Any other drivers need to be installed?
I tried these steps in win10/win11, it doesn't work on both system.
0 Kudos
Reply

7,058 Views
frank_m
Senior Contributor III

You are not by chance using VMs, and forgot to connect USB device(s) forth and back between host and VM ?

Here an example of a connected STM eval board, with the integrated debugger reflashed to a Segger J-Link:

frank_meyer_0-1686750783126.png

 

0 Kudos
Reply

7,054 Views
ZJane
Contributor I
not VMs, I try to configure the board on two computers(one pc with win10 and another with win11) and encounter the same problem.
maybe other drivers should be installed?
0 Kudos
Reply

7,047 Views
frank_m
Senior Contributor III

I only occasionally use an LPC board on a Windows10 PC (LPCxpresso54628 board).
LPC-Link driver installation was part of the LPCXpresso IDE installation, and worked mostly fine for me.
I have no experience with Win11.

I hope the NXP staff can help you in this regard.

0 Kudos
Reply

7,044 Views
ZJane
Contributor I
Thanks all the same.
0 Kudos
Reply