arm-uclinuxeabi- have same problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

arm-uclinuxeabi- have same problem

1,509件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by hujiafu on Thu Mar 24 06:59:23 MST 2016
I was porting the lpc1788 on uclinux. and use arm-uclinuxeabi-gcc
when I porting minigui, it used libc.a and libpthread.a, but it caused SEVG error.
finally I found the libc.a and libpthread.a compilered as ARM code (32bit), but Lpc1788 is based on cortex-m3, it's only support Thumb code (16 bit), so I must compiler libc and libpthread by myself.
However the glibc check my cross toolchain and reported the arm-uclinuxeabi-ld is too old.
my toolchain is arm-2010q1-uclinux .
1. can any one have new version toolchain for uclinux ?
2. the  arm-uclinuxeabi-gcc is used uclibc or glibc ?
can any one help me?
thank you !!!
ラベル(1)
0 件の賞賛
返信
1 返信

1,375件の閲覧回数
lpcware
NXP Employee
NXP Employee
bump
0 件の賞賛
返信