adc_8xx.h trigger sources in SEQ_CTRL

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

adc_8xx.h trigger sources in SEQ_CTRL

ソリューションへジャンプ
2,035件の閲覧回数
vaque
Contributor II

Hi!;

I am working about a LPC824. In order to use the ADC with LPCOPEN I have to trigger it with the SCT.

At this time, adc_8xx.h macro in "ADC hardware trigger sourcers in SEQ_CTRL" are 11 items. These 11 items aren't like the ADC hardware trigger inputs (Table276. ADC hardware trigger inputs) in UM10800.pdf. These item aren't similiar at all.

I am confused. Is the macro other thing?.

Thanks so much and regards. Daniel.

ラベル(2)
0 件の賞賛
返信
1 解決策
1,921件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Daniel Vaquerizo,

Firstly, the Table 276 exemplifies the correct hardware trigger inputs, you can ignore the interference as LPCOpen library is designed for all kinds of LPC MCU, and the LPCOpen for the LPCXpresso 824 would inherit  all macro certainly.

Hope this is clear.
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,922件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Daniel Vaquerizo,

Firstly, the Table 276 exemplifies the correct hardware trigger inputs, you can ignore the interference as LPCOpen library is designed for all kinds of LPC MCU, and the LPCOpen for the LPCXpresso 824 would inherit  all macro certainly.

Hope this is clear.
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
1,921件の閲覧回数
vaque
Contributor II

Ok. Thanks. Have a great day too

Regards. Daniel.

0 件の賞賛
返信