about ADC

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

about ADC

2,975 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by sanjeevudupi on Tue May 07 05:21:40 MST 2013

hello all,


i am using LPC4333FET256 for our project. in ADC driver we are using ADC0_2/ADC1_2 decicated ADC pin,


at the same time, from muti functionality pins, i am making use of ADC0_2(from PF_8 pin) and ADC1_2(from PF_9 pin).


from ADC pin select registers(SCU) "ENAIO0" register , i can select ADC0_2 and from "ENAIO1"  i can select ADC1_2 


but i am facing problem in selecting the dedicated pin. 


from which register, i can select dedicated pin ie ADC0_2/ADC1_2.


see page num 233, i attached user manual


thanks in advance


 


regards


sanjeevudupi

Labels (1)
0 Kudos
Reply
1 Reply

2,818 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Jg on Tue May 28 03:57:52 MST 2013

The ADC0_x and ADC1_x input channels are always tied together. You cannot use them as dedicated pins. So although both ADC0/1 have 8 input channels the total number of separate channels is also 8, not 2x8.

0 Kudos
Reply