Writing internal EEPROM from within a fault exception

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Writing internal EEPROM from within a fault exception

1,350件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by stewo on Tue Dec 09 10:00:29 MST 2014
Hello,

is it possible to write to the internal EEPROM of LPC4078 from within a fault exception handler? We tried but it seems not to work, so I'd like to know if it's generally impossible or if I'm doing something wrong.

Thanks
ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,260件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by stewo on Wed Dec 10 01:26:12 MST 2014
I wrote my own driver which polls the interrupt status register (busy waiting) to detect when the write operation has finished. So it's not interrupt based if that's the question. The driver works well during regular operation but it hangs when I try to write from within a fault handler.
0 件の賞賛
返信

1,260件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by TheFallGuy on Tue Dec 09 11:40:37 MST 2014
How are you writing to the EEPROM?
0 件の賞賛
返信