Will FRO_HF trun off FRO_12M?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Will FRO_HF trun off FRO_12M?

2,441 Views
da_chen
Contributor II

I am using lpc54114. I found in SDK, when we use

CLOCK_SetupFROClocking(12000000)

It will turn off FRO_HF.

I wonder if we turn on FRO_HF, the FRO_12M will be turned off of not?

Labels (1)
0 Kudos
Reply
3 Replies

2,337 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Da Chen,

"if we turn on FRO_HF, the FRO_12M will be turned off of not?"

-> Yes, it will turned off. Only can choose one of them as input:

pastedImage_3.png

pastedImage_1.png

Hope it helps,

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply

2,337 Views
da_chen
Contributor II

Hi Alice_Yang,

Thanks for your replying.

But how can you tell the fro working status just from the picture you provided? MAINCLKSELA is just for choosing clock source, right? Although the fro_hf is chosen as the input? Can't the fro_12m still running?

Da Chen

0 Kudos
Reply

2,337 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Da Chen,

Sorry I misunderstood your meaning.

Yes, the FRO_12M still running, there is no register that disable this clock in LPC54114.

Hope it helps,

TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply