Why USBHost_Mass_Storage is so slow on LPC1788,LPC1850

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Why USBHost_Mass_Storage is so slow on LPC1788,LPC1850

1,194 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by whoms on Sat Apr 28 17:51:11 MST 2012
I've tested nxpUSBLib 0.94 on LPC1788,LPC1850. USB flash disk is directly sector wrote using USBHost_Mass_Storage .
The speed is only 150KB/s. And I've verified the LPC1850's USB0 host is set at High Speed mode.
LPC1788 is running at 108MHz,USB CLK=48MHz
LPC1850 is running at 167MHz,USB CLK=480MHz

Can anybody give an explanation ? How to improve the USB flash disk writing speed to about 1MB/s on LPC185x or LPC435x ?
标签 (1)
0 项奖励
回复
0 回复数