Which series is LPC1114F/301?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Which series is LPC1114F/301?

1,219 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by sposnjak on Tue Jun 25 14:38:49 MST 2013

I am confused about which series is LPC1114F/301 01.134 ZSD09 470AY? First I thought that is LPC11XXLV now I think that is LPC11XX? Does anybody know? Thank you.

Labels (1)
0 Kudos
Reply
1 Reply

1,181 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by starblue on Wed Jun 26 01:00:09 MST 2013

It is just an ordinary LPC1114, see the ordering information in the data sheet or user manual.


The F specifies temperature range, in other series (e.g. LPC43xx) there may also be a J there for a wider range. Normally you would only write it together with the part specifying the package, i.e. LPC1114FBD48/301.


BTW, I dislike that some of the LPC11xx series are distinguished only by the /nnn suffix, that makes them hard to search for. A common prefix for each series would be much better.

0 Kudos
Reply