Which LWIP?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Which LWIP?

1,861 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by ntipping on Wed Oct 23 09:42:20 MST 2013
Hi All,

I'm just looking into using LWIP. When I find my way to the LWIP page, it informs me that I should be using the LPCOpenversion 'here'. When I follow the link, it takes me to the LPCOpen page, where there are links to LWIP, which take me back to where I started. Can anyone please advise?

Thanks in advance.

Nick Tipping
Labels (1)
0 Kudos
Reply
2 Replies

1,821 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by ntipping on Thu Oct 24 06:55:37 MST 2013
Dear Wells,

Thanks for clarifying that.

Best Regards,

Nick Tipping
0 Kudos
Reply

1,821 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by wells on Wed Oct 23 16:57:00 MST 2013
Yes, that is a bit confusing. LWIP is included as part of the LPCOpen releases now instead of a standalone package with the need to download older code bundles.

You will need to download the v1.03 release in the legacy LPCOpen v1.xx section. (http://www.lpcware.com/system/files/lpcopen_v1.03.zip)
There are projects in there for Keil, IAR, and LPCXpresso for using LWIP for the 1768, 1788, 4088, 18xx, and 43xx.

LPCOpen v1.03 can be a bit overwhelming. Some documentation to get started is here: http://docs.lpcware.com/lpcopen/v1.03/
(The installation notes and v1.xx quickstart guides will apply to you for v1.03)
0 Kudos
Reply