Which IDE, LPCXpresso or MCUXpresso ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Which IDE, LPCXpresso or MCUXpresso ?

ソリューションへジャンプ
2,247件の閲覧回数
anaseem
Contributor IV

User Manual says LPC11E68JBD48E is ARM Cortex-M0+ based.

Following is note from NXP Website:

NOTE: MCUXpresso IDE is now recommended for developers using LPC Cortex-M based microcontrollers.

Please confirm that LPC11E68JBD48E is not Cortex-M based ?

ラベル(1)
1 解決策
2,079件の閲覧回数
converse
Senior Contributor V

Use MCUXpresso. LPC11xxx is a Cortex-M device.

元の投稿で解決策を見る

2 返答(返信)
2,079件の閲覧回数
soledad
NXP Employee
NXP Employee

Hi,

I suggest to use MCUXpresso.

MCUXpresso IDE contains built in support for a slightly extended set of LPC Cortex-M based parts that were supported in LPCXpresso IDE v8.2.2.
LPC Cortex-M include Cortex-M0+ devices.

MCUXpresso IDE supports the LPC11E68JBD48


Have a great day,

Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

2,080件の閲覧回数
converse
Senior Contributor V

Use MCUXpresso. LPC11xxx is a Cortex-M device.