Where is the GUIDRV_Page1bpp.h driver header file?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Where is the GUIDRV_Page1bpp.h driver header file?

1,397件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by rhaguiuda on Fri Jul 18 05:59:04 MST 2014
I cannot find the driver header file GUIDRV_Page1bpp in current emWin distribuition. Only GUIDRV_SPage is provided.

Where is the GUIDRV_Page1bpp located? Is it missing?
ラベル(1)
0 件の賞賛
返信
1 返信

1,267件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by mc on Fri Jul 18 19:47:00 MST 2014
Hi rhaguiuda,
These drivers are compile time driver. Which NXP emWin library version did you see these drivers and which version you did not see?
You can request Segger. See below link.
http://www.segger.com/emwin-guidrv-page1bpp.html
0 件の賞賛
返信