When is the next update scheduled for?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

When is the next update scheduled for?

2,386件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by mjm46 on Wed Feb 29 14:19:21 MST 2012
Do you have an updated estimate for the next USB LIB release, also will the missing iso endpoint configuration functionality be added for the LPC11U14 in this next release?

Best Regards,

Mike
ラベル(1)
  • USB

0 件の賞賛
返信
6 返答(返信)

2,378件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by equinox on Tue May 22 06:52:37 MST 2012
When is full support for lpc43xx going to be added to the library?
Will my Hitex LPC4350 board be supported?
When can we expect version 1.0 to be released?
0 件の賞賛
返信

2,378件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by nxpUSBlib team on Mon Mar 19 21:42:13 MST 2012
v0.93 will be out this Thursday.

FYI This release will include an experimental CMSIS driver for the LPC43xx which compiles but is not hooked up. All examples for the LPC43xx use the LPC18x CMSIS. We will have native support for the M4 in the v0.94 release which is planned for release in 4 weeks.
0 件の賞賛
返信

2,378件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by equinox on Mon Mar 19 13:40:06 MST 2012
So is the release supposed to be out right around now? Or has it been pushed back?
I need support for my hitex lpc4300 dev board.
Specifically the USB mass storage host example.
0 件の賞賛
返信

2,378件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by nxpUSBlib team on Fri Mar 02 14:14:30 MST 2012
Yes it will eventually. It will be runnable on either core. We also plan to add support for both controllers simultaneously.
0 件の賞賛
返信

2,378件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by dima2611 on Fri Mar 02 11:23:40 MST 2012
Will the LPC43xx family become a "full member" of the library?
0 件の賞賛
返信

2,378件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by nxpUSBlib team on Fri Mar 02 10:30:43 MST 2012
We hope to get the next release out in two weeks. Isochronous support for the LPC11Uxx family will not be in this release but we do have it planned in the near future, perhaps as early as the release after this one.
0 件の賞賛
返信