What is the external extended SRAM recommended device for the LPC2378

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

What is the external extended SRAM recommended device for the LPC2378

1,405件の閲覧回数
liuzichang007
Contributor I

What is the external extended SRAM recommended device for the LPC2378 (the SRAM capacity should be less than 128KB as much as possible)? How to design its hardware and drive? Is there a reference design?

ラベル(1)
0 件の賞賛
返信
1 返信

1,298件の閲覧回数
CarlosCasillas
NXP Employee
NXP Employee

Hi,

The evaluation/reference board for LPC2378 (LPC2378-STK) doesn’t include external RAM chip, although it has External Memory Bus.

As reference, you could take a look to Olimex LPC2294 board (LPC-L2294) that uses the K6R4016V1D SRAM:

https://www.olimex.com/Products/ARM/NXP/LPC-L2294-1MB/


Hope this will be useful for you.
Best regards!
/Carlos

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信