VirtualSerial driver has code 10 under windows 7

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

VirtualSerial driver has code 10 under windows 7

1,468件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by marshall on Thu Sep 13 07:48:47 MST 2012
The VirtualSerial example runs on the board, and shows in usbview.exe. But installing the .inf file that is in the VirtualSerial Example makes windows 7 64bit say that it cannot start the driver with a code 10. I saw another thread about this topic, but the poster just said that he fiddled with the .inf file and it now works, does anyone know what fiddling (exactly) needs to be done?

Thanks.
ラベル(1)
  • USB

0 件の賞賛
返信
1 返信

1,452件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by marshall on Thu Sep 13 14:08:40 MST 2012
I gave up on the driver supplied with the Example_VirtualSerial and just installed another CDC driver, it appears to work, at least sometimes. So unless anyone has any input on why the nxp driver doesn't work then I have moved on to the next bug. :)
0 件の賞賛
返信