Using the SRAM only

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Using the SRAM only

868 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by wafa on Mon Mar 25 00:52:47 MST 2013
Hi,

I'm fairly new to programming microcontrollers; I've been working with the LPC1788 for a couple of weeks now.
One problem I've been having recently is that P3.xx (full modem signals)can be connected to RS232 interface only if 16-bit databus version used, or i have a 32 MB SDRAM with a 32-bit databus width on the eval board.
The only solution i found is to use the on-chip memory only but i couldn't find the way to control the memory allocation.

Thanks.
Labels (1)
0 Kudos
Reply
0 Replies