Using the LPC54608 for senior design project: Virtual Drum

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Using the LPC54608 for senior design project: Virtual Drum

1,684 次查看
andrewliu
Contributor I

Our senior design project was to create a virtual drum.

Digital Drum - Dem boys - YouTube 
Here's a short video demonstration of the final design in action.

The input is a cheap piezoelectric microphone, which transmits the signals to the LPCXpresso 54608 board. The board is used to read the data (mainly the intensity of each hit) and output a snare drum sound corresponding the intensity of the hit.

I've attached the report for our final design, with an explanation of how the code works.

The code can be found here: Demboys/README.md at master · hwebin/Demboys · GitHub

0 项奖励
回复
1 回复

1,598 次查看
soledad
NXP Employee
NXP Employee

Hi Andrew,

Thank you for your input.

Regards

Sol

0 项奖励
回复