Using LPC1788FBD208K for a new design with a 7" TFT

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Using LPC1788FBD208K for a new design with a 7" TFT

1,241 次查看
MartinEnG
Contributor II

Hello,

I'm integrating an LPC1788FBD208K into a new product. I'll use the MCU to directly control a 7" TFT LCD screen with a 24-bit RGB interface. I can see that the MCU does have a specialized module for TFT screen control, but I haven't been able to find any tool that allows me to design GUIs easily. I searched through the GUI Guider documentation, but it seems it's not compatible with the MCU I want to use. Do you have any tools I could use to create the GUI more easily? I really wouldn't want to have to program all the graphical windows myself, and I might even consider using another MCU that has a TFT LCD controller module if necessary to use GUI Guider or LVGL with MCUXpresso SDK

Regards,

Walter.

0 项奖励
回复
1 回复

1,232 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

As you know that the LPC1788 is a bit old, it was launched in 2013 year.

The GUI guider does not support the LPC1788, if you want to use GUI guider tools to develop graphic interface, I suggest you consider LPC54xxx including LPC54628, LPC54018 which have LCD interface and GUI guider supports the two chips.

Hope it can help you

BR

XiangJun Rong

0 项奖励
回复