Using LPC1788 Color-Lookup-Table with emWin

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Using LPC1788 Color-Lookup-Table with emWin

927件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by abcxyz on Thu May 31 01:39:06 MST 2012
Hello

Im trying to use the Color-Lookup-Table of the LPC1788 with emWin.

I use the Embedded-Artist-Evalbord. The idea is not to use external memory in the endproduct.I placed the VRAM memory in the internal memory, but id dont understand how to config the emWin Library to work with the color-lookup table of the LPC1788. I even dont know if the GUI-Driver delivered with the BSP of this Page does support this method.





ラベル(1)
0 件の賞賛
返信
0 返答(返信)