Use pin 2.9 as RXD for Uart2 (Lpc1769)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Use pin 2.9 as RXD for Uart2 (Lpc1769)

1,982 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Scorpio on Tue Nov 26 03:35:45 MST 2013
Can anybody to help me? I try to use the pin 2.9 as RXD for the uart 2 (Lpc1769). I use Lpcopen and setup pin in function mode (2), as input and initialize at state low. I connect the data out from a rfid module but the interrupt of uart is never fired up. If i use the same rfid module and config the pin 0.11 as RXD, everything works perfectly.
标签 (1)
0 项奖励
回复
4 回复数

1,940 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Pacman on Wed Nov 27 10:28:10 MST 2013
What was the problem ?
0 项奖励
回复

1,940 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Scorpio on Wed Nov 27 03:22:22 MST 2013
Thank you very much. I found the solution.
0 项奖励
回复

1,940 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Scorpio on Tue Nov 26 23:38:41 MST 2013
Hi mc,

I use the LPC1769 LPCXpresso board separately for testing. I need this pin to work for a customized board of our company. If i drive the pin at ground for a moment i can get the interrupt from the uart (2). Then i can see some data at my uart buffer. 
0 项奖励
回复

1,940 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by mc on Tue Nov 26 23:08:17 MST 2013
Hi Scorpio,
Are you using our evaluation board or you have your own customized board?
0 项奖励
回复