Unused xtal pins

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Unused xtal pins

1,465 Views
richardsoennich
Contributor I

Does NXP offer any guidelines on what to do with unused xtal pins?  (LPC1114)

Thanks

Rich

0 Kudos
Reply
1 Reply

1,347 Views
soledad
NXP Employee
NXP Employee

Hi Rich,

When the system oscillator is not used, connect XTALIN and XTALOUT as follows: XTALIN can be left floating or can be grounded (grounding is preferred to reduce susceptibility to noise). XTALOUT should be left floating.

I hope this helps,


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply