Unused pin in LPC11C14

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Unused pin in LPC11C14

1,342 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by jhd on Tue Feb 02 08:39:45 MST 2016
Hello,

The unused pin of LPC11C14, I can leave the disconnected if I will not use?  Or they need to be pulled?

Best regards

Labels (1)
0 Kudos
Reply
2 Replies

1,327 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by jhd on Wed Feb 03 04:43:36 MST 2016
Thanks very much!.

Regards

EDIT:  In LPC15xx datasheet, chapter 14.7 page 93 it's explained everything. "Termination of unused pins".
0 Kudos
Reply

1,327 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by 1234567890 on Tue Feb 02 10:11:47 MST 2016
Unused pins should be left unconnected and configurated as input with internal pull-up or pull-down enabled to avoid floating.
0 Kudos
Reply