Unable to program LPC1547 using Flash Magic

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Unable to program LPC1547 using Flash Magic

1,631 Views
gouthamuttarkar
Contributor I

Crystal 16MHz

Hex file 8KB

I am using USB UART Bridge to program LPC1547 

I have successfully programmed it two days ago and now it's causing problems.

The microcontroller is not responding to "?" For autobaud 

Tags (2)
0 Kudos
Reply
1 Reply

1,513 Views
soledad
NXP Employee
NXP Employee

Hi,

Please try with an ISP reset,  check the following thread,

https://community.nxp.com/thread/389040 


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply