USBMidi on LPC2478

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

USBMidi on LPC2478

1,541件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by jdeas on Wed Apr 10 08:59:08 MST 2013

This is my first visit to LPCware and I am not seeing much in the way of LCP2478 projects. Currently I am using some IAR code to run my USB project but moving into MIDI is a bit different. What code base (if any) are supplied here that I can port over to the 2478 processor? I assume that many of the blocks in this device match those in other LPC series.

ラベル(1)
  • USB

0 件の賞賛
返信
1 返信

1,500件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by boston on Mon May 20 08:55:10 MST 2013

Sorry, I can't help you on LPC2478, have you made any progress since your post?  I'm using LPC17xx and the USBlib works on that. The library has MIDI code, but no MIDI examples. Do you know how to use the MIDI functions in library? If so I'd be grateful if you could share some example code. Thanks and good luck.

0 件の賞賛
返信