USBD init() and uninit()

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

USBD init() and uninit()

835 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Idanba on Thu Mar 19 06:26:02 MST 2015
Hi,

Looking at the examples supplied I can clearly see the init() routine through all the interfaces supplied by the stack( USBD_API->hw->Init, USBD_API->cdc->init etc.)
but, I don't understand what shall I do in case I'd like to uninit the stack and stop its operation ?
If I want to use another ( different ) USB SW stack with the same USB resource I'm currently working through USBD stack, what do I need to do in order to stop the operation of the USBD stack?

Thanks in advance,
Idan
Labels (1)
0 Kudos
Reply
0 Replies