USBD ROM stack: CDC class NCM support

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

USBD ROM stack: CDC class NCM support

Jump to solution
2,925 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by ZZZMQP on Sat Mar 19 17:19:22 MST 2016
Hello,

I'm looking for NCM support (Ethernet-over-USB) for the CDC class. Does anyone have any information if this is supported in the USBD ROM stack directly, or where to get it?

Cheers,
  Dusty.
Labels (1)
0 Kudos
Reply
1 Solution
2,708 Views
ckphua
NXP Employee
NXP Employee

This is not supported in USB Device ROM stack.

View solution in original post

0 Kudos
Reply
3 Replies
2,708 Views
ckphua
NXP Employee
NXP Employee

This is not supported in USB Device ROM stack.

0 Kudos
Reply
2,708 Views
gregdunn
Contributor I

Any luck with adding NCM support?

Thanks,

Greg

0 Kudos
Reply
2,708 Views
lpcware
NXP Employee
NXP Employee
bump
0 Kudos
Reply