USB pins as a general purpose pins in LPC1342

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

USB pins as a general purpose pins in LPC1342

1,341件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by grzegorzw on Mon Jun 15 03:17:43 MST 2015
I am writing to ask about a possibility to use USB pins in LPC 1342 as a general purpose pins.
I would like to use USB_DM and USB_DP pins as a outputs to control external device.
I would like to ask it is possible ?and if it is. How can I set this pin as output.
Thank for reply.
ラベル(1)
0 件の賞賛
返信
1 返信

1,271件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by R2D2 on Mon Jun 15 03:30:27 MST 2015
User manual:


Quote:
On LPC134x, [color=#f00]PIO3_4 and PIO3_5 are not available[/color]. The corresponding pins are used for the USB D+ and D− functions.

0 件の賞賛
返信