USB mass storage with SD card

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

USB mass storage with SD card

2,150 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by inspire on Sun Sep 20 06:04:55 MST 2015
Hi,

I'm looking for a LPC43xx project with LPCOpen that allows using a SD card as a USB mass storage.

In the LPCOpen version 1.03 I could find an example project called "ngx_xplorer_4330_usblib_device" which is exactly what I'm looking for - but with an old LPCOpen version. Before rewriting everything for LPCOpen 2.xx, is there a similar example for the LPCOpen 2.xx library? There is none in the LPCOpen 2.xx versions I downloaded...Maybe someone else has developed this? :)

Thanks!
inspire
Labels (1)
0 Kudos
Reply
2 Replies

1,749 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by inspire on Thu Sep 24 06:23:06 MST 2015
Awesome, thanks a lot, mc!
0 Kudos
Reply

1,748 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by mc on Mon Sep 21 09:05:00 MST 2015
Hi inspire,
Please try attached LPCxpresso project for LPC1837. It is very easy to port it to LPC4300. It is using ROM based USB driver not LPCUSBLib though.
0 Kudos
Reply