USB ROM and MSC with removable devices and multiple LUNs

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

USB ROM and MSC with removable devices and multiple LUNs

1,107 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by mubes on Sat Apr 12 04:32:21 MST 2014
Folks,

I'm using the LPC13Uxx USB ROM to implement a composite device, one element of which is a MSC driver.

Unfortunately the MSC is talking 'through' to a SD card which could, on occasion, not be present, or could be removed during operation...it could also be replaced with another one I guess. I also have some on-board memory that it would be nice to export on a separate LUN.  The 'default' MSC handler (header in mw_usbd_mscuser.h) is a simple in/out affair that doesn't seem to cope with these scenarios.

Intriguingly, there is the facility to incorporate a custom Ep0 handler and the SCSI definitions too (in MSC_CTRL_T) which I suspect can be used to do what I need without having to hack up an entire stack.

So, the question is; can anyone point me in the right direction for examples or documentation to do such a thing?  There's a _lot_ of docs around for the usb stuff, but it all seems a big mass to someone just wading through this...

Thanks in advance for any help anyone can offer.

Regards

DAVE
Labels (1)
0 Kudos
Reply
0 Replies