USB ROM API in LPC4370

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

USB ROM API in LPC4370

1,783 Views
hmyoong
Contributor III

Chapter 27: "LPC43xx/LPC43Sxx USB API" of the LPC43xx user's manual states that the USB ROM API is only available for LPC4350/30/20 and LPC43S50/S30/S20 parts.  However, the LPCOpen libraries and examples for LPC4370 include examples for usbd_rom_xxxxx.  Please advise.

Labels (3)
Tags (1)
0 Kudos
Reply
1 Reply

1,377 Views
hmyoong
Contributor III

Let me answer my own question, after reading the code and cross checked using Google's search 

Code:

By looking at the labtool/fw/Lib_USB/LPCUSBLIB/LPCUSBlibConfig.h

// Define USE_USB_ROM_STACK = 1 to use MCU's internal ROM stack, 0 if otherwise

#define USB_FORCED_FULLSPEED 0

Google's search 

http://www.nxp-lpc.com/images/nxpUSBlib_v1_1.pdf

It is confirmed that LPC4370 does not support USB ROM API.