USB OTG on LPC54606 ?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

USB OTG on LPC54606 ?

1,695 次查看
gph
Contributor III

Hi,

Is it possible to use USB On The Go on LP54606 ?

I don't find any schematic and not really response in user manual.

Thanks a lot.

Philippe.

标签 (1)
标记 (1)
0 项奖励
回复
1 回复

1,601 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi Philippe GRAILLE,

Thank you for your interest in NXP Semiconductor products and
for the opportunity to serve you.
Q1) Is it possible to use USB On The Go on LP54606 ?
-- No, so I'd recommend you to consider using the LPC43xx series to replace the LP54606.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复