USB OTG on LPC54606 ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

USB OTG on LPC54606 ?

1,765 Views
gph
Contributor III

Hi,

Is it possible to use USB On The Go on LP54606 ?

I don't find any schematic and not really response in user manual.

Thanks a lot.

Philippe.

Labels (1)
Tags (1)
0 Kudos
Reply
1 Reply

1,671 Views
jeremyzhou
NXP Employee
NXP Employee

Hi Philippe GRAILLE,

Thank you for your interest in NXP Semiconductor products and
for the opportunity to serve you.
Q1) Is it possible to use USB On The Go on LP54606 ?
-- No, so I'd recommend you to consider using the LPC43xx series to replace the LP54606.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply