URGENT HELP with lpc1769 mass erase

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

URGENT HELP with lpc1769 mass erase

838 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by pindonga123 on Thu Oct 31 15:08:51 MST 2013
Hello. I couldnt debug in my lpc1769. I put true value in the vector catch and it worked. But i cant do a mass erase. Appear the next legend
Pc: (  0) Reading remote configuration
Ni: LPCXpresso Debug Driver v4.0 (May 21 2012 21:42:41)
Nc: Looked for chip XML file in C:/nxp/LPCXpresso_4.2.3_292/lpcxpresso/bin/LPC1769.xml

Nc: Looked for vendor directory XML file in C:/nxp/LPCXpresso_4.2.3_292/lpcxpresso/bin/nxp_directory.xml

Nc: Found generic directory XML file in C:/nxp/LPCXpresso_4.2.3_292/lpcxpresso/bin/crt_directory.xml

Pc: (  5) Remote configuration complete
Pc: ( 30) Emulator Connected
Pc: ( 40) Debug Halt
Pc: ( 50) CPU ID
Nc: Emu(0): Conn&Reset. DpID: 2BA01477. Info: T1S6RGRIA
Nc: SWD Frequency: 250 KHz. RTCK: False. Vector catch: False.
Nc: Packet delay: 0  Poll delay: 0.
Nc: NXP: LPC1769  Part ID: 0x26113F37
Pc: ( 65) Chip Setup Complete
Nt: Connected: was_reset=false. was_stopped=false
Cr:v Registered license, download limit of 128K
Pc: ( 70) License Check Complete
Nt: Mass Erase
Ed:04: Failed to erase flash: Ef(9). Flash erase or write operation aborted.
Pc: (100) Target Connection Failed
What can be?
Labels (1)
0 Kudos
Reply
1 Reply

803 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Thu Oct 31 15:27:32 MST 2013
Please try the suggestions on the FAQ:
http://www.lpcware.com/content/faq/lpcxpresso/regaining-debug-access

BTW: LPCXpresso v4 is very out of date now. I'd recommend upgrading the LPCXpresso 6:
http://www.lpcware.com/lpcxpresso/home
0 Kudos
Reply