Two image(frimware) on LPC1830

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Two image(frimware) on LPC1830

1,593件の閲覧回数
kensu
Contributor V

Dears

If I need run two firmware with LPC1830, and the compiler is use MCUXpresso,

After I jump to second image, is it possible that I can still use step by step to debug with LPC Link?

For first image, it can use step by step on MCUXpresso, after I copy second image to another ram(Ex: SDRAM) by image1.

I want to know if I can debug with step by step?

My flow will be like:

Image1: Run some application and copy image2 from Flash to SDRAM and jump to image2.

iamge2: Run second application.

Thank you

Ken

ラベル(2)
0 件の賞賛
返信
1 返信

1,495件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Ken Su ,

Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
1) After I jump to the second image, is it possible that I can still use step by step to debug with LPC Link?
-- No, I'm afraid not.


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信