Tips for dual core performance on LPC55S69?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Tips for dual core performance on LPC55S69?

1,864件の閲覧回数
scottm
Senior Contributor II

I thought I saw an app note on optimizing dual-core performance on the LPC55S6x family, but I can't find anything now.

Does such a resource exist? What I'm mostly looking for is information on memory contention. I see that both cores share the same flash memory interface. What kind of performance is achievable with both cores running from flash? Does the second core need to be running from RAM to be useful?

Thanks!

0 件の賞賛
返信
3 返答(返信)

1,848件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi scottm 

For LPC55 dual core communication, I suggest you referring "LPC55xx/LPC55Sxx Dual Core Communication"

https://www.nxp.com.cn/docs/en/application-note/AN12335.pdf

and "LPC55xx/LPC55Sxx Dual-Core Debug in MCUXpresso"

https://www.nxp.com.cn/docs/en/application-note/AN12358.pdf

Hope this helps,

Jun Zhang

 

 

0 件の賞賛
返信

1,800件の閲覧回数
scottm
Senior Contributor II

Hi Jun,

I've read those, and AN12335 does mention running code from an alternate RAM bank for best performance.

What I'm looking for is more information on how to structure things when it's not feasible to run the whole thing from RAM, and what kind of performance hit I can expect. I don't see anything at all in NXP's docs about running both cores from flash, but I'm sure I've seen information somewhere about using both cores with FreeRTOS and I don't think that involved completely separate copies of the RTOS.

This seems like a big topic that ought to have a lot of discussion somewhere. If it's not in NXP's documentation, is there ARM documentation I should be reading instead?

Thanks,

Scott

0 件の賞賛
返信

1,791件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

HI scottm 

I don't think this is a NXP documentation.

Thanks,

Jun Zhang

 

0 件の賞賛
返信