The Initial Status of LPC11C24

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

The Initial Status of LPC11C24

1,618 次查看
rasheedkhankan
Contributor II

Hello,

When we buy a new a single chip LPC11C24, what is the status of its flash memory???

1. without boatloader??? In this case how can I flash it??

2. Or with booatloader???

Thanks in advance,

Rasheed

标签 (4)
0 项奖励
回复
1 回复

1,524 次查看
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Rasheed,

The MCUs come with a blank FLASH memory from the factory but please notice that the LPC11C24 MCUs have also a ROM memory with a bootloader that controls initial operation after reset and also provides the means to accomplish programming of the flash memory via UART or C_CAN.


Hope it helps!

Best Regards,
Carlos Mendoza
Technical Support Engineer

0 项奖励
回复