Target Reset Pattern

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Target Reset Pattern

Jump to solution
1,793 Views
lb_h
Contributor I

Hello,all

Can the I3C module of the LPC55xx family of chips send a "Target Reset Pattern" through a configuration register?Whether the T-bit of the I3C command is automatically calculated by the hardware or can be configured by software.

Labels (1)
0 Kudos
Reply
1 Solution
1,759 Views
Harry_Zhang
NXP Employee
NXP Employee

Hi @lb_h 

In the LPC55xx family, the I3C module does not have a dedicated configuration register to directly send the “Target Reset Pattern.” However, it supports sending custom command sequences, which can be used to generate the reset pattern manually by software.

The T-bit is typically calculated automatically by the hardware based on the I3C command.

BR

Harry

View solution in original post

0 Kudos
Reply
1 Reply
1,760 Views
Harry_Zhang
NXP Employee
NXP Employee

Hi @lb_h 

In the LPC55xx family, the I3C module does not have a dedicated configuration register to directly send the “Target Reset Pattern.” However, it supports sending custom command sequences, which can be used to generate the reset pattern manually by software.

The T-bit is typically calculated automatically by the hardware based on the I3C command.

BR

Harry

0 Kudos
Reply