System clock

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

System clock

1,474 Views
zhan8g
Contributor I

It is found that there is a problem in the LPC54102 chip. The internal IRC 12MHz clock is passed through EMI, but IRC has the problem of temperature drift. The long-term usage leads to UART communication rate deviation and can not communicate. Using 32K RTC PLL TO 12MHz, the system clock temperature drift problem has been solved, but there are more serious problems and very poor anti-interference. Why does this chip have such a problem?!!

Labels (1)
0 Kudos
Reply
1 Reply

1,374 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,

Thank you for your interest in NXP Semiconductor products and 
the opportunity to serve you.

I'd like to get the more detailed information about this issue, so whether you can introduce the process of testing and tell me the device revision number of this LPC54102 chip.

Have a great day.

TIC
 
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
0 Kudos
Reply