Standalone programming options for LPC54618

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Standalone programming options for LPC54618

4,602件の閲覧回数
gmk1
Contributor III

Hardware I have - 

  • PE Multilink Universal and custom LPC54618J512BD208 board

I want to download hex file to board using above hardware using some standalone tools.

I cannot use FlashMagic due to hardware restrictions.

Of course I can do with MCUXpresso or Keil but those are complete IDE which is not an option for me.

Any standalone tools if available on internet please suggest!?

I'm open to buy new hardware if such tools exist.

Regards, Gmk

ラベル(2)
0 件の賞賛
返信
6 返答(返信)

4,419件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi, 

Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
1) Any standalone tools if available on the internet please suggest!?
-- I'd like to suggest you can consider the Cyclone series product and you can learn the more detail information about it via going through the below links.
1. http://www.pemicro.com/products/product_viewDetails.cfm?product_id=15320165&productTab=1
2. http://www.pemicro.com/products/product_viewDetails.cfm?product_id=15320167&productTab=1

Have a great day,

TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信

4,419件の閲覧回数
gmk1
Contributor III

jeremyzhou‌

Thanks for the reply.

They look promising but looks like very costly solution.

Do we have any other alternatives?

0 件の賞賛
返信

4,419件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi ,

Thanks for your reply.
The SmartPRO 5000U-PLUS programmer is designed by a Chinese company:ZLG, maybe you can consider it.

Have a great day,

TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信

4,419件の閲覧回数
gmk1
Contributor III

Hi and thanks for replying...

I cannot procure Chinese products at my workplace for some reasons.

Do you know any software tools like Flashmagic which works with PE Micro Universal/LPC Link etc.?

0 件の賞賛
返信

3,551件の閲覧回数
hxlong911
Contributor I

https://www.chinaobd2.com/wholesale/smartpro-5000u-plus-universal-usb-programmer-3059.html

smartpro 5000u-plus, is a very good programmer, you can try it.

0 件の賞賛
返信

4,419件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi,

Thanks for your reply.
I'd like you to use the J-Flash Lite tool in the SEGGER as the below shows.

pastedImage_1.png

Have a great day,

TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信