Some problems getting started

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Some problems getting started

1,235件の閲覧回数
maza
Contributor I

Hello!

In my company was working some employee who destroyed the LPCXpresso824 max board that I'm using now and of course, its giving me some headaches.

To begin, I tried to build and load the blink example but didn't work. Then I realize that I probably should reflash the firmware by updating a new binary file... okey, tried an didn't work. I pressed the reset button while pluggin in the usb connector but nothing happens and my devide manager doesn't detect anything, is this right? Shouldn't the device manager show a new device called CRP DISABLD as the guide says?

To make it easier, it's my very first time programming MCU, not counting Arduino. So i'm too lost to start without any help.

Could you help me? 

Thanks

0 件の賞賛
返信
1 返信

1,145件の閲覧回数
soledad
NXP Employee
NXP Employee

Hi, 

Please check the following link, you will find a way to recover the board getting it into ISP mode.

Regaining debug access to target MCU 

Have a great day,
Sol

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信