Sample code for GUITDRV_ADS7846 new Library

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Sample code for GUITDRV_ADS7846 new Library

1,825件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by econfalonieri on Tue Oct 01 03:55:51 MST 2013
I'm in need to find some sample code / examples using the new emWin Library (post 5.16) with the GUITDRV_ADS7846 for the touch controller ADS7846/TSC2046 that is mounted on the LPC4088 Embedded Artist Eval Board.
May some of you help?
All the examples available use the old generic Touch library that is not working well...
ラベル(1)
0 件の賞賛
返信
1 返信

1,617件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by mc on Wed Oct 02 06:52:38 MST 2013
Hi,
Did you already try below BSP?
http://www.lpcware.com/content/nxpfile/emwin-522-board-support-package-ea1788-board
0 件の賞賛
返信