STOP ALL INTERRUPTS

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

STOP ALL INTERRUPTS

1,245 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by brattchess on Wed Mar 18 02:36:43 MST 2015
Hello,

It would be possible to stop all interrupts using some register? Or I need to stop all enabled source interrupts and when I need to enable these to manage the source interrupts one by one?
I would like to know it because I am using the IAP commands to use the flash.
Labels (1)
0 Kudos
Reply
2 Replies

1,235 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by brattchess on Wed Mar 18 03:24:07 MST 2015
You are OK!!
Thanks.
0 Kudos
Reply

1,235 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by R2D2 on Wed Mar 18 03:05:30 MST 2015
What's wrong with  __disable_irq()  :quest:
0 Kudos
Reply