SSP/SSEL and GPIO pin interrupt

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SSP/SSEL and GPIO pin interrupt

1,009 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by capiman on Fri Mar 20 14:36:28 MST 2015
Hello,

does someone know if it is possible to execute a GPIO pin interrupt even when pin is configured for SSP/SSEL?
I need SSEL for SSP slave functionality but want to trigger an interrupt when SSEL goes high and low...

Best regards,

Martin
Labels (1)
0 Kudos
Reply
1 Reply

952 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by R2D2 on Fri Mar 20 16:46:24 MST 2015

Quote: capiman
does someone know if it is possible to execute a GPIO pin interrupt even when pin is configured for SSP/SSEL?



Just try it  :)

With LPC11xx it's possible (to generate an PIN interrupt with PIN function SLAVE / SSEL) :O
0 Kudos
Reply